Other Parts Discussed in Thread: DM3730, OMAP3530
Hi All,
I have tested OMAP3530/DM3730 TVOUT display,when it bring up show the problem as write line in the picture .But for LCD&VGA display is ok.So any advice for this issue.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shulev,
The venc.c below the mail,i'm not sure it case the error.h
[ 593.995086] VENC_F_CONTROL 00000000
[ 594.000732] VENC_VIDOUT_CTRL 00000001
[ 594.006378] VENC_SYNC_CTRL 00000040
[ 594.011718] VENC_LLEN 0000035f
[ 594.017578] VENC_FLENS 00000270
[ 594.023193] VENC_HFLTR_CTRL 00000000
[ 594.028533] VENC_CC_CARR_WSS_CARR 2f7225ed
[ 594.034332] VENC_C_PHASE 00000000
[ 594.039947] VENC_GAIN_U 00000130
[ 594.045562] VENC_GAIN_V 000001b0
[ 594.050903] VENC_GAIN_Y 000001b0
[ 594.056701] VENC_BLACK_LEVEL 0000003b
[ 594.062316] VENC_BLANK_LEVEL 0000003b
[ 594.067657] VENC_X_COLOR 00000007
[ 594.073455] VENC_M_CONTROL 00000002
[ 594.079071] VENC_BSTAMP_WSS_DATA 0000003f
[ 594.084686] VENC_S_CARR 2a098acb
[ 594.090026] VENC_LINE21 00000000
[ 594.095825] VENC_LN_SEL 01290015
[ 594.101440] VENC_L21__WC_CTL 0000f603
[ 594.106781] VENC_HTRIGGER_VTRIGGER 00000000
[ 594.112548] VENC_SAVID__EAVID 06a70108
[ 594.118194] VENC_FLEN__FAL 00180270
[ 594.123809] VENC_LAL__PHASE_RESET 00040135
[ 594.129150] VENC_HS_INT_START_STOP_X 00880358
[ 594.134918] VENC_HS_EXT_START_STOP_X 000f035f
[ 594.140533] VENC_VS_INT_START_X 01a70000
[ 594.145874] VENC_VS_INT_STOP_X__VS_INT_START_Y 000001a7
[ 594.151672] VENC_VS_INT_STOP_Y__VS_EXT_START_X 01af0000
[ 594.157287] VENC_VS_EXT_STOP_X__VS_EXT_START_Y 000101af
[ 594.162902] VENC_VS_EXT_STOP_Y 00000025
[ 594.168243] VENC_AVID_START_STOP_X 03530083
[ 594.174041] VENC_AVID_START_STOP_Y 026c002e
[ 594.179656] VENC_FID_INT_START_X__FID_INT_START_Y 0001008a
[ 594.185180] VENC_FID_INT_OFFSET_Y__FID_EXT_START_X 002e0138
[ 594.191223] VENC_FID_EXT_START_Y__FID_EXT_OFFSET_Y 01380001
[ 594.197113] VENC_TVDETGP_INT_START_STOP_X 00140001
[ 594.202728] VENC_TVDETGP_INT_START_STOP_Y 00010001
[ 594.208068] VENC_GEN_CTRL 00ff0000
[ 594.213897] VENC_OUTPUT_CONTROL 0000000d
[ 594.219512] VENC_OUTPUT_TEST 00000000
I test the TV out on my board but here is I don't observe such problem. Give me same info about your board - are you using beagle board or some custom board? Which software and version you are using?
BR
Tsvetolin Shulev