This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Active Hyperlink boot on C6678



Hi all,

We are currently planning to use the C6678 in combination with an Altera FPGA. Both are connected via Hyperlink. The FPGA will have a flash-device attached, but we don't want to add a second flash for the DSP.

Now we are thinking about using Hyperlink-boot in the DSP. But in opposite to the mechanism implemented in the RBL we'd like to use "active"-, non host-mode. Thus, after initialization of the core and the Hyperlink-connection the DSP shall load an ELF-file - might be something else too - from a Hyperlink-region directly into his internal memory. The advantage of this approach is, that we could load a large linux-image directly into the attached ddr memory without having to use another bootloader stage.

Do you have any concerns regarding this mechanism?

Is there a way to achieve this?

Am I right that I cannot use and extend the IBL because it won't fit into the eeprom of the device (next to the RBL?), thus making it neccessary to attach a flash-device (which is what we don't want to do)?

Is there are way to modify the RBL? Especially considering that everthing is already either inside the RBL (Hyperlink-, and other initialization stuff) or inside the IBL (ELF-file parsing/loading). I already found out that TI want publish the source code of the RBL so it might be an option for TI to add a parameter (Bootloader-IOs) for the Hyperlink-boot to load an elf from a fixed address after getting a Hyperlink-IRQ and reading a magic-code on some hyperlink-address.

Looking forward to your suggestions.

Thanks

Andreas Oetken