Other Parts Discussed in Thread: DM3730
TI Team,
I was wondering if I could get the complete register map for the USB OTG module on the DM3730. Also, would it be possible to get obtain the source code for the bootloader?
-David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DM3730
TI Team,
I was wondering if I could get the complete register map for the USB OTG module on the DM3730. Also, would it be possible to get obtain the source code for the bootloader?
-David
David,
You'll not get the BOOT ROM code from anywhere. It is internal to TI. You can refer to x-loader or u-boot code if required. There is USB enough code available in u-boot which initialized USB. Also you can refer to an Android boot loader where Android fast boot is used. It uses USB gadget drivers for fast boot.
TI Team,
I don't know, what information is covered in the "non-public" version of the TRM for the DM3730. Is it possible to see the complete non-public version ?
If I have the be very specific, then I have an immediate need for the for the complete register map and description for the USB OTG module including the "Mentor" registers. The TRM gives only the "TI specific" registers. Also, if there is any chance to get access to the source code of the bootloader, that would be very helpful. I'm especially interested in the USB portion of the bootloader.
David,
Eventhough I'm not a TI employee, I may be able to answer your questions.
Since the USB controller is from Mentor Graphics, I don't think you'll be able to get the MUSB controller documents easily. There is not TI document available for the MUSB IP. The document is basically available from Mentor. Please refer the below links for more info.
http://processors.wiki.ti.com/index.php/Inventra_HDRC_USB_Controller
http://www.design-reuse.com/news/187/mentor-graphics-dual-role-ip-core-full-speed-usb-2-0-standard-go-portable-specification.html