This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 AVI file decode error



When I use DM368 to decode the AVI file in H.264 format, the AVI file is 1080P 30fps.

DM368 used ARM clock 486 MHz, DDR clock 360 MHz, and sensor clock 74.25MHz as VENC clock.

File read from USB storage and decode the AVI file into YUV420 format , then resize to 1080P 30fps for VPBE output .

The playback AVI file can't reach 1080P 30fps, the VGA display is miss some frames.

Can I decode AVI file then resize to 1080P 30fps as VPBE output ?

If I can decode the file, do I need to use which one decode version and which one PDK version ?