From a previous discussion I gather that the current codec user guide is incorrect when it says XDM_RESET is not supported on the speech codecs. So, my customer is now trying to use XDM_RESET with G.729 speech decoder.
They tried doing XDM_RESET on the decoder in the middle of processing an audio stream, that is between two encoded frames, then it takes several frames before the decoder will produce a good output. So, is this the way to handle packet losses or should they do something else when dealing with that?
By the way, the XDM_REset documentation issue will need to be fixed in G.729, G.722 and iILBC user guides.
Rgds
-Dipa-