hi,
i have met such problem that when i use aac encode(lc-aac)in dvsdk4,i set the bit-rate and sample-rate as 64000,44100 in Params,dynParams.the encode works well.but i increase the bit-rate as 96000,this occured Failed to create audio encoder: aaclcenc.and i change into default Params(the bitrate is 128000 and sample-rate is 44100),it couldn't work too.
when i use the demo in dvsdk ,it uses default Params(samplerate if 44100,bitrate is 128000),it does not work ,when i change the bitrate to 64000,it works,what is wrong with it?
so i cant find the reason and solve it ,can anyone help me ?thanks very much.