This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Could someone tell me which file the defination of function snd_pcm_open is in used in the dvsdk4.0?Thank you!

Could someone tell me which file the defination of function snd_pcm_open is in used in the dvsdk?As shows in the following picture, Sound_alsa_create in the path of  dami_2_20_00_15\packages\ti\sdo\dmai\linux calls "snd_pcm_open",then where is the defination of funciton "snd_pcm_open" in the dvsdk?

Thank you!