Other Parts Discussed in Thread: TMS320C6713B
Hello, I have a question. Now I use EDMA+MCBSP with TMS320C6713B to link AIC23B and send data to headphone. When I have hardware emulation, there is no problem and the result is perfect. But when I load the hex file in the external FLASH, it has problems.
First, I have three DSP boards, but only one board can run rightly, in other boards the EDMA will not come into the ISR.(I have two leds to test. One led test the timer0's ISR, the other which is not flash test EDMA's interrupt ) I am sure the AIC23B is set rightly. I have looked the wave through the OSC.
Second, the board which runs rightly will be channel swapping sometimes.
The configuration I am using is the following:
#include <stdio.h>
#include <string.h>
#include <stdlib.h>
#include <math.h>
#include <ctype.h>
//CSL
#include <csl.h>
#include <csl_cache.h>
#include <csl_edma.h>
#include <csl_timer.h>
#include <csl_irq.h>
#include <csl_mcbsp.h>
#include <csl_edma.h>
……
short gBufferXmtPing[BUFFSIZE]; // Transmit PING buffer
short gBufferXmtPong[BUFFSIZE]; // Transmit PONG buffer
……
#define PING 0
#define PONG 1
EDMA_Handle hEdmaXmt; // EDMA channel handles
EDMA_Handle hEdmaReloadXmtPing;
EDMA_Handle hEdmaReloadXmtPong;
short gXmtChan;
unsigned char xmtdone = 0 ;
short pingORpong=PING;
/* Transmit side EDMA configuration */
EDMA_Config gEdmaConfigXmt = {
EDMA_FMKS(OPT, PRI, HIGH) | // Priority
EDMA_FMKS(OPT, ESIZE, 16BIT) | // Element size
EDMA_FMKS(OPT, 2DS, NO) | // 2 dimensional source?
EDMA_FMKS(OPT, SUM, INC) | // Src update mode
EDMA_FMKS(OPT, 2DD, NO) | // 2 dimensional dest
EDMA_FMKS(OPT, DUM, NONE) | // Dest update mode
EDMA_FMKS(OPT, TCINT, YES) | // Cause EDMA interrupt?
EDMA_FMKS(OPT, TCC, OF(0)) | // Transfer complete code
EDMA_FMKS(OPT, LINK, YES) | // Enable link parameters?
EDMA_FMKS(OPT, FS, NO), // Use frame sync?
(Uint32)&gBufferXmtPing, // Src address
EDMA_FMK (CNT, FRMCNT, NULL) | // Frame count
EDMA_FMK (CNT, ELECNT, BUFFSIZE), // Element count
EDMA_FMKS(DST, DST, OF(0)), // Dest address
EDMA_FMKS(IDX, FRMIDX, DEFAULT) | // Frame index value
EDMA_FMKS(IDX, ELEIDX, DEFAULT), // Element index value
EDMA_FMK (RLD, ELERLD, NULL) | // Reload element
EDMA_FMK (RLD, LINK, NULL) // Reload link
};
void initEdma(void)
{
/* Configure transmit channel */
hEdmaXmt = EDMA_open(EDMA_CHA_XEVT0, EDMA_OPEN_RESET); // get hEdmaXmt handle and reset channel
hEdmaReloadXmtPing = EDMA_allocTable(-1); // get hEdmaReloadXmtPing handle
hEdmaReloadXmtPong = EDMA_allocTable(-1); // get hEdmaReloadXmtPong handle
gEdmaConfigXmt.dst = MCBSP_getXmtAddr(hMcbsp0); // set the desination address to McBSP1 DXR
gXmtChan = EDMA_intAlloc(-1); // get an open TCC
gEdmaConfigXmt.opt |= EDMA_FMK(OPT,TCC,gXmtChan); // set TCC to gXmtChan
EDMA_config(hEdmaXmt, &gEdmaConfigXmt); // then configure the registers
EDMA_config(hEdmaReloadXmtPing, &gEdmaConfigXmt); // and the reload forPing
gEdmaConfigXmt.src = EDMA_SRC_OF(gBufferXmtPong); // change the structure to have a source of Pong
EDMA_config(hEdmaReloadXmtPong, &gEdmaConfigXmt); // and configure the reload for Pong
EDMA_link(hEdmaXmt,hEdmaReloadXmtPong); // link the regs to Pong
EDMA_link(hEdmaReloadXmtPong,hEdmaReloadXmtPing); // link Pong to Ping
EDMA_link(hEdmaReloadXmtPing,hEdmaReloadXmtPong); // and link Ping to Pong
/* Enable interrupts in the EDMA controller */
EDMA_intClear(gXmtChan);
EDMA_intEnable(gXmtChan); // enable EDMA interrupts (CIER)
EDMA_enableChannel(hEdmaXmt); // enable EDMA channel
/* Do a dummy write to generate the first McBSP transmit event */
MCBSP_write(hMcbsp0, 0);
}
/* McBSP codec data channel configuration */
static MCBSP_Config mcbspCfg0 = {
MCBSP_FMKS(SPCR, FREE, NO) |
MCBSP_FMKS(SPCR, SOFT, NO) |
MCBSP_FMKS(SPCR, FRST, YES) |
MCBSP_FMKS(SPCR, GRST, YES) |
MCBSP_FMKS(SPCR, XINTM, XRDY) |
MCBSP_FMKS(SPCR, XSYNCERR, NO) |
MCBSP_FMKS(SPCR, XRST, YES) |
MCBSP_FMKS(SPCR, DLB, OFF) |
MCBSP_FMKS(SPCR, RJUST, RZF) |
MCBSP_FMKS(SPCR, CLKSTP, DISABLE) |
MCBSP_FMKS(SPCR, DXENA, OFF) |
MCBSP_FMKS(SPCR, RINTM, RRDY) |
MCBSP_FMKS(SPCR, RSYNCERR, NO) |
MCBSP_FMKS(SPCR, RRST, YES),
MCBSP_FMKS(RCR, RPHASE, SINGLE) |
MCBSP_FMKS(RCR, RFRLEN2, DEFAULT) |
MCBSP_FMKS(RCR, RWDLEN2, DEFAULT) |
MCBSP_FMKS(RCR, RCOMPAND, MSB) |
MCBSP_FMKS(RCR, RFIG, NO) |
MCBSP_FMKS(RCR, RDATDLY, 0BIT) |
MCBSP_FMKS(RCR, RFRLEN1, OF(1)) |
MCBSP_FMKS(RCR, RWDLEN1, 16BIT) |
MCBSP_FMKS(RCR, RWDREVRS, DISABLE),
MCBSP_FMKS(XCR, XPHASE, SINGLE) |
MCBSP_FMKS(XCR, XFRLEN2, DEFAULT) |
MCBSP_FMKS(XCR, XWDLEN2, DEFAULT) |
MCBSP_FMKS(XCR, XCOMPAND, MSB) |
MCBSP_FMKS(XCR, XFIG, NO) |
MCBSP_FMKS(XCR, XDATDLY, 0BIT) |
MCBSP_FMKS(XCR, XFRLEN1, OF(1)) |
MCBSP_FMKS(XCR, XWDLEN1, 16BIT) |
MCBSP_FMKS(XCR, XWDREVRS, DISABLE),
MCBSP_FMKS(SRGR, GSYNC, DEFAULT) |
MCBSP_FMKS(SRGR, CLKSP, DEFAULT) |
MCBSP_FMKS(SRGR, CLKSM, DEFAULT) |
MCBSP_FMKS(SRGR, FSGM, DEFAULT) |
MCBSP_FMKS(SRGR, FPER, DEFAULT) |
MCBSP_FMKS(SRGR, FWID, DEFAULT) |
MCBSP_FMKS(SRGR, CLKGDV, DEFAULT),
MCBSP_MCR_DEFAULT,
MCBSP_RCER_DEFAULT,
MCBSP_XCER_DEFAULT,
MCBSP_FMKS(PCR, XIOEN, SP) |
MCBSP_FMKS(PCR, RIOEN, SP) |
MCBSP_FMKS(PCR, FSXM, EXTERNAL) |
MCBSP_FMKS(PCR, FSRM, EXTERNAL) |
MCBSP_FMKS(PCR, CLKXM, INPUT) |
MCBSP_FMKS(PCR, CLKRM, INPUT) |
MCBSP_FMKS(PCR, CLKSSTAT, DEFAULT) |
MCBSP_FMKS(PCR, DXSTAT, DEFAULT) |
MCBSP_FMKS(PCR, FSXP, ACTIVEHIGH) |
MCBSP_FMKS(PCR, FSRP, ACTIVEHIGH) |
MCBSP_FMKS(PCR, CLKXP, FALLING) |
MCBSP_FMKS(PCR, CLKRP, RISING)
};
void initMcbsp0()
{
/* Open the codec data McBSP */
hMcbsp0 = MCBSP_open(MCBSP_DEV0, MCBSP_OPEN_RESET);
/* Configure the codec to match the AIC23 data format */
MCBSP_config(hMcbsp0, &mcbspCfg0);
/* Start the McBSP running */
MCBSP_start(hMcbsp0, MCBSP_XMIT_START | MCBSP_RCV_START |
MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC, 220);
}
void initMcbsp1()
{
……
}
void main(){
CSL_init(); /* initialize the CSL library */
DEVCFG = 0x0;
Init_PLL(); /*initialize PLL*/
Init_EMIF(); /*initialize emif */
for(i=0;i<BUFFSIZE;i++)
{
gBufferXmtPing[i] = 0 ;
gBufferXmtPong[i] = 0 ;
}
initMcbsp0();
initMcbsp1();
……
IRQ_globalDisable(); /* Disable all interrupts */
initEdma();
IER=1; /* Disable all interrupts except NMI */
IRQ_setVecs((void *)0x800); /* point to the IRQ vector table */
ICR = 0x0ffff ;
IER |= 0x4133; /*enable EXINT4 EXINT5 TIME0 EDMA interrupt*/
IRQ_globalEnable(); /*enable all interrupts*/
……
while(1)
{
……
}
}
Thanks a lot for your time.
Regards,
HTS