This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ARM will not boot Linux: hwclock: can't open '/dev/misc/rtc'



Hi

I have an evm that uses the TCI6614 processor. The ARM core has been booting Linux with no problems, but today it will not boot.

Please take a look at the following console listing and suggest what may be the problem.

BR

David

Please wait: booting...

Starting udev

udevd (407):

/proc/407/oom_adj is deprecated, please use /proc/407/oom_score_adj instead.

alignment: ignoring faults is unsafe on this CPU.  Defaulting to fixup mode.

Root filesystem already rw, not remounting

Caching udev devnodes

Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory

logger: mount: mount point /proc/bus/usb does not exist

NOT configuring network interfaces: / is an NFS mount

net.ipv4.conf.default.rp_filter = 1

net.ipv4.conf.all.rp_filter = 1 kernel.core_uses_pid = 1

kernel.core_pattern = core-%e-%s-%u-%g-%p-%t

fs.suid_dumpable = 2

hwclock: can't open '/dev/misc/rtc': No such file or directory

Wed Aug 29 18:39:00 UTC 2012

hwclock: can't open '/dev/misc/rtc': No such file or directory

eth0: no IPv6 routers present

keystone-rapidio 2900000.rapidio: RIO port register timeout, ports 00000001 not ready