This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6657 Spi workaround



Hi,

  I found a spi workaround to access CS0 from the 80 pin header from this e2e thread:  http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/212050/752026.aspx

Will this workaround cause my NAND boot to now not work.  I realize the NOR boot is now not possible.

Thanks,

Will

  • Will,

    The EVM modification described in the other thread allows use of the SPI port over the 80-pin expansion connector.  This modification disables the on-board SPI NOR FLASH device.  This has no impact on the on-board NAND FLASH device attached to the Async EMIF-16 bus.

    Tom