Other Parts Discussed in Thread: TMS320F28335, SM320C6727B
We have a control application where a TMS320F28335 is not providing enough computation throughput. It is an extended temperature application so we are looking at SM32C6713B or SM320C6727B processors. The SM320C6727B is only available up to 250MHz in the extended temperature range while the SM32C6713B is 300MHz.
A few questions:
1) Any idea how much faster on average the x6700 family would be over the 150MHz '335? It does have a clock rate advantage plus a significantly wider computational path.
2) The SM32C6727B seems to have an improved memory and cache architecture. Would this be enough to offset it being 50MHz slower in our temperature range?