Hi, all
I develop on dm8168 evm board with vs card using dvrrdk 2.80,
i want to capture audio using tvp5158, and i run the dvrrdk demo
but now when my kernel start ,
i see that
ALSA device list:
No soundcards found,
-----------------
later i run the demo
ALSA lib pcm_hw.c:1401:(_snd_pcm_hw_open) Invalid value for card
AUDIO >> Cannot open audio device plughw:0,0 (No such file or directory)
AUDIO: Capture -> device init failed....- exiting!!!!!
how can the kernel find no ALSA devices ?
Is there any modify should be done in kernel menuconfigure,
i also see the kernel menucfg , all driver has attached ?
bestregards
xavier