This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMDM6467 load and debug



I am using EVMDM6467 with CCS V5. I have got XDS 510 USB Plus.

1) I have set the boot mode pin to "Emulator mode"(0000). I have selected the example project by name LED. Whenever I try to debug,  a dialog box by name "Spectrum Digital XDS 510USB Emulator_0/IcePick_C_0" will pop up stating "Error initializing emulator". I wanted to debug the project line by line. Even if I choose the other example projects which has come along with EVMDM6467, it is the same case.

2) I had tried to load "i2c_eeprom_writer.out" as given under A.4.1 of  "User Guide for EVMDM6467". I was not able to load "i2c_eeprom_writer.out".

[For MSP430, I have used the same CCS V5 compiler. I am able to debug and load the program.]

Please get me a way to debug and load the program for EVMDM6467.