Other Parts Discussed in Thread: DM3730
Hi,
We are working on DM3730 based BeaglexM Board. We are new gstreamer and DSP.
We installed DVSDK 4.01 in BeaglexM Board.
We were able to play local video file (320x240@30fps , 1280x720@30fps ) using gstreamer.
Similarly we are able to play smoothly network stream video file of resolution 1280x720@30fps on DVI interface.
But, when we are streaming an video files of resolution 320x240@30fps, the display is not smooth. It is playing for 2-3 seconds and then stopping for other 2-3 seconds and playing.....
We had used the following command for decoding:
gst-launch -v udpsrc uri="udp://192.168.1.40:5544" ! mpegtsdemux ! queue ! h264parse ! TIViddec2 ! tidisplaysink2
With the same command we are able to play smoothly input stream video of resolution 1280x720@30fps.
We tried with TIDmaiVideoSink element also......but still the same.
Host Side:
We are streaming an TS file (video of resolution 320x240@ 30 fps MPEG-TS encapsulation) using VLC Player.
Help us in resolving this issue.
Regards
SudhirKumar.Reddipalli