This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x serial port access

Hi everybody, I'm using am335x development kit with default O.S. and u-boot. The board is configured to profile 1, and I'm trying to communicate with one of serial ports. Bellow is my /dev directory. The Wiki page says that profile 1 uses the J10 DB9 connector, but I didn't find a device in /dev linked to J10 DB9 connector.

Besides, the only serial port that works is J12 DB9 conector in the main board, accessed in (/dev/ttyO1). But, that J12 DB9 conector redirect all received bytes to the terminal. Could someone help me in this issue? What /dev/ttyX need I use to access 1 of the 5 serial ports? If I need configure a /dev device, what archive need I change and how can I proceed?

drwxr-xr-x 2 root root 620 Jan 1 2000 block
drwxr-xr-x 3 root root 60 Jan 1 2000 bus
drwxr-xr-x 2 root root 2040 Apr 11 08:27 char
crw------- 1 root root 5, 1 Apr 11 08:27 console
crw-rw---- 1 root root 10, 61 Jan 1 2000 cpu_dma_latency
drwxr-xr-x 6 root root 120 Jan 1 2000 disk
crw-rw-rw- 1 root root 1, 7 Jan 1 2000 full
crw-rw---- 1 root root 89, 1 Jan 1 2000 i2c-1
prw------- 1 root root 0 Jan 1 2000 initctl
drwxr-xr-x 2 root root 60 Jan 1 2000 input
crw-r----- 1 root kmem 1, 2 Jan 1 2000 kmem
crw-rw---- 1 root root 1, 11 Jan 1 2000 kmsg
srw-rw-rw- 1 root root 0 Apr 11 08:27 log
crw-rw---- 1 root root 10, 237 Jan 1 2000 loop-control
brw-rw---- 1 root disk 7, 0 Jan 1 2000 loop0
brw-rw---- 1 root disk 7, 1 Jan 1 2000 loop1
brw-rw---- 1 root disk 7, 2 Jan 1 2000 loop2
brw-rw---- 1 root disk 7, 3 Jan 1 2000 loop3
brw-rw---- 1 root disk 7, 4 Jan 1 2000 loop4
brw-rw---- 1 root disk 7, 5 Jan 1 2000 loop5
brw-rw---- 1 root disk 7, 6 Jan 1 2000 loop6
brw-rw---- 1 root disk 7, 7 Jan 1 2000 loop7
crw-r----- 1 root kmem 1, 1 Jan 1 2000 mem
brw-rw---- 1 root floppy 179, 0 Jan 1 2000 mmcblk0
brw-rw---- 1 root floppy 179, 1 Jan 1 2000 mmcblk0p1
brw-rw---- 1 root floppy 179, 2 Jan 1 2000 mmcblk0p2
brw-rw---- 1 root floppy 179, 3 Jan 1 2000 mmcblk0p3
brw-rw---- 1 root floppy 179, 4 Jan 1 2000 mmcblk0p4
crw-rw---- 1 root root 10, 60 Jan 1 2000 network_latency
crw-rw---- 1 root root 10, 59 Jan 1 2000 network_throughput
crw-rw-rw- 1 root root 1, 3 Jan 1 2000 null
crw-rw---- 1 root root 10, 1 Jan 1 2000 psaux
crw-rw-rw- 1 root root 5, 2 Apr 11 10:56 ptmx
drwxr-xr-x 2 root root 0 Jan 1 1970 pts
brw-rw---- 1 root disk 1, 0 Jan 1 2000 ram0
brw-rw---- 1 root disk 1, 1 Jan 1 2000 ram1
brw-rw---- 1 root disk 1, 10 Jan 1 2000 ram10
brw-rw---- 1 root disk 1, 11 Jan 1 2000 ram11
brw-rw---- 1 root disk 1, 12 Jan 1 2000 ram12
brw-rw---- 1 root disk 1, 13 Jan 1 2000 ram13
brw-rw---- 1 root disk 1, 14 Jan 1 2000 ram14
brw-rw---- 1 root disk 1, 15 Jan 1 2000 ram15
brw-rw---- 1 root disk 1, 2 Jan 1 2000 ram2
brw-rw---- 1 root disk 1, 3 Jan 1 2000 ram3
brw-rw---- 1 root disk 1, 4 Jan 1 2000 ram4
brw-rw---- 1 root disk 1, 5 Jan 1 2000 ram5
brw-rw---- 1 root disk 1, 6 Jan 1 2000 ram6
brw-rw---- 1 root disk 1, 7 Jan 1 2000 ram7
brw-rw---- 1 root disk 1, 8 Jan 1 2000 ram8
brw-rw---- 1 root disk 1, 9 Jan 1 2000 ram9
crw-rw-rw- 1 root root 1, 8 Jan 1 2000 random
crw-rw---- 1 root root 10, 63 Jan 1 2000 rfkill
lrwxrwxrwx 1 root root 4 Jan 1 2000 rtc -> rtc0
crw-rw---- 1 root audio 254, 0 Jan 1 2000 rtc0
drwxrwxrwx 2 root root 40 Jan 1 2000 shm
drwxr-xr-x 2 root root 60 Jan 1 2000 snd
crw-rw-rw- 1 root root 5, 0 Jan 1 2000 tty
crw--w---- 1 root root 4, 0 Jan 1 2000 tty0
crw--w--w- 1 root root 4, 1 Apr 11 08:27 tty1
crw--w---- 1 root root 4, 10 Jan 1 2000 tty10
crw--w---- 1 root root 4, 11 Jan 1 2000 tty11
crw------- 1 root root 4, 12 Apr 11 10:47 tty12
crw--w---- 1 root root 4, 13 Jan 1 2000 tty13
crw--w---- 1 root root 4, 14 Jan 1 2000 tty14
crw--w---- 1 root root 4, 15 Jan 1 2000 tty15
crw--w---- 1 root root 4, 16 Jan 1 2000 tty16
crw--w---- 1 root root 4, 17 Jan 1 2000 tty17
crw--w---- 1 root root 4, 18 Jan 1 2000 tty18
crw--w---- 1 root root 4, 19 Jan 1 2000 tty19
crw--w---- 1 root root 4, 2 Jan 1 2000 tty2
crw--w---- 1 root root 4, 20 Jan 1 2000 tty20
crw--w---- 1 root root 4, 21 Jan 1 2000 tty21
crw--w---- 1 root root 4, 22 Jan 1 2000 tty22
crw--w---- 1 root root 4, 23 Jan 1 2000 tty23
crw--w---- 1 root root 4, 24 Jan 1 2000 tty24
crw--w---- 1 root root 4, 25 Jan 1 2000 tty25
crw--w---- 1 root root 4, 26 Jan 1 2000 tty26
crw--w---- 1 root root 4, 27 Jan 1 2000 tty27
crw--w---- 1 root root 4, 28 Jan 1 2000 tty28
crw--w---- 1 root root 4, 29 Jan 1 2000 tty29
crw--w---- 1 root root 4, 3 Jan 1 2000 tty3
crw--w---- 1 root root 4, 30 Jan 1 2000 tty30
crw--w---- 1 root root 4, 31 Jan 1 2000 tty31
crw--w---- 1 root root 4, 32 Jan 1 2000 tty32
crw--w---- 1 root root 4, 33 Jan 1 2000 tty33
crw--w---- 1 root root 4, 34 Jan 1 2000 tty34
crw--w---- 1 root root 4, 35 Jan 1 2000 tty35
crw--w---- 1 root root 4, 36 Jan 1 2000 tty36
crw--w---- 1 root root 4, 37 Jan 1 2000 tty37
crw--w---- 1 root root 4, 38 Jan 1 2000 tty38
crw--w---- 1 root root 4, 39 Jan 1 2000 tty39
crw--w---- 1 root root 4, 4 Jan 1 2000 tty4
crw--w---- 1 root root 4, 40 Jan 1 2000 tty40
crw--w---- 1 root root 4, 41 Jan 1 2000 tty41
crw--w---- 1 root root 4, 42 Jan 1 2000 tty42
crw--w---- 1 root root 4, 43 Jan 1 2000 tty43
crw--w---- 1 root root 4, 44 Jan 1 2000 tty44
crw--w---- 1 root root 4, 45 Jan 1 2000 tty45
crw--w---- 1 root root 4, 46 Jan 1 2000 tty46
crw--w---- 1 root root 4, 47 Jan 1 2000 tty47
crw--w---- 1 root root 4, 48 Jan 1 2000 tty48
crw--w---- 1 root root 4, 49 Jan 1 2000 tty49
crw--w---- 1 root root 4, 5 Jan 1 2000 tty5
crw--w---- 1 root root 4, 50 Jan 1 2000 tty50
crw--w---- 1 root root 4, 51 Jan 1 2000 tty51
crw--w---- 1 root root 4, 52 Jan 1 2000 tty52
crw--w---- 1 root root 4, 53 Jan 1 2000 tty53
crw--w---- 1 root root 4, 54 Jan 1 2000 tty54
crw--w---- 1 root root 4, 55 Jan 1 2000 tty55
crw--w---- 1 root root 4, 56 Jan 1 2000 tty56
crw--w---- 1 root root 4, 57 Jan 1 2000 tty57
crw--w---- 1 root root 4, 58 Jan 1 2000 tty58
crw--w---- 1 root root 4, 59 Jan 1 2000 tty59
crw--w---- 1 root root 4, 6 Jan 1 2000 tty6
crw--w---- 1 root root 4, 60 Jan 1 2000 tty60
crw--w---- 1 root root 4, 61 Jan 1 2000 tty61
crw--w---- 1 root root 4, 62 Jan 1 2000 tty62
crw--w---- 1 root root 4, 63 Jan 1 2000 tty63
crw--w---- 1 root root 4, 7 Jan 1 2000 tty7
crw--w---- 1 root root 4, 8 Jan 1 2000 tty8
crw--w---- 1 root root 4, 9 Jan 1 2000 tty9
crw------- 1 admin tty 253, 0 Apr 11 09:54 ttyO0
crw-rw---- 1 root dialout 253, 1 Jan 1 2000 ttyO1
crw-rw---- 1 root dialout 253, 2 Jan 1 2000 ttyO2
crw-rw---- 1 root dialout 253, 3 Jan 1 2000 ttyO3
crw-rw---- 1 root dialout 253, 4 Jan 1 2000 ttyO4
crw-rw---- 1 root dialout 253, 5 Jan 1 2000 ttyO5
crw-rw---- 1 root root 10, 62 Jan 1 2000 ubi_ctrl
-rw-r--r-- 1 root root 8 Jan 1 2000 udev_network_queue
crw-rw-rw- 1 root root 1, 9 Jan 1 2000 urandom
crw-rw---- 1 root tty 7, 0 Jan 1 2000 vcs
crw-rw---- 1 root tty 7, 1 Jan 1 2000 vcs1
crw-rw---- 1 root tty 7, 12 Apr 11 08:27 vcs12
crw-rw---- 1 root tty 7, 128 Jan 1 2000 vcsa
crw-rw---- 1 root tty 7, 129 Jan 1 2000 vcsa1
crw-rw---- 1 root tty 7, 140 Apr 11 08:27 vcsa12
crw-rw---- 1 root root 10, 130 Jan 1 2000 watchdog
crw-rw-rw- 1 root root 1, 5 Jan 1 2000 zero

thanks in advanced.