Dear support,
I ran the wizard to check "Notify" functionality. I am confused about the event ID and Interrupt being used in the example
Event ID 10 is register in the C6670 manual to be a memory protection fault (section 7.9.1 table 7.38)
I though that interrupt could only be from INT4 to INT15
IsNotify_registerEvent completely separated from the Event mapping and Interrupt used in Hwi_create?
Thanks for the clarification
Aymeric