This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP4 ABE BT_VX Switch Configuration in WinCE 7

All,

We are working on a WinCE 7 based platform which is having OMAP4430.

We have BT Chipset connected over McBSP2. In Linux world, we enable the "DL1 Mixer" and the ""DL1 BT_VX Switch" to provide output on the BT-VX DL Port. Can anybody please point out the equivalent support/code-base for the OMAP4 Windows CE BSP?

We are using the OMAP4 WinCE BSP version W24.26.

Thanks,
Ravindra