This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Concetro Instrumentation

HI, 

I want to log some variables from the concerto DSP to the host, I am having a 1 ms timer, I wanted to know how many variables can i log in 1 ms if i configure, how can i calculate this,will this be the desired configuration LoggingSetup to JTAG run-mode and ServiceMgr to Topology_SINGLECORE,TransportType_FILE.

  • Hi Shadab,

    Just a heads-up...use TransportType_FILE writes a file onto your host. Which core are you trying to do the logging? M3 or C28? Are you using TI-RTOS (also called MCUSDK)? If you are, there is an example of using LoggerIdle over USB to System Analyzer.

    Todd