Other Parts Discussed in Thread: OMAP3530
Hi ,
I am working on OMAP 3530 Processor (ARM Cortex-A8 processor+C64x DSP) based our own development kit. I am trying to enable dsplink in-order to make DSP to work.
I have followed the steps given in the http://ossie.wireless.vt.edu/trac/wiki/BeagleBoard_DSPLink web link. I could able to build and insert dsplinkk.ko file successfully. But while running the sample application i am getting below kernel panic errors.
root@ULK:~#
root@ULK:~#
root@ULK:~# insmod dsplinkk.ko
[ 62.337951] DSPLINK Module (1.61.03) created on Date: Dec 5 2012 Time: 15:53:18
root@ULK:~# insmod lpm_omap3530.ko
root@ULK:~# ./lpmON.x470uC
==== LPM ON Test ====
app: LPM_open
app: LPM_set(LPM_CTRL_REFCOUNTOVR)
app: LPM_on
app: LPM_close
==== All Done ====
root@ULK:~# ./lpmOFF.x470uC
==== LPM OFF Test ====
app: LPM_open
app: LPM_set(LPM_CTRL_REFCOUNTOVR)
app: LPM_off
app: LPM_close
==== All Done ====
root@ULK:~# ./messagegpp message.out 1000
========== Sample Application : MESSAGE ==========
Entered MESSAGE_Create ()
[ 131.886535] Unable to handle kernel paging request at virtual address 31362e51
[ 131.894226] pgd = c7de4000
[ 131.896972] [31362e51] *pgd=00000000
[ 131.900634] Internal error: Oops: 5 [#1] PREEMPT
[ 131.905273] Modules linked in: lpm_omap3530 dsplinkk nls_iso8859_1 ircomm_tty ircomm irda
[ 131.913574] CPU: 0 Not tainted (2.6.29-omap1 #18)
[ 131.918823] PC is at PMGR_PROC_load+0x140/0x244 [dsplinkk]
[ 131.924438] LR is at PMGR_PROC_load+0xec/0x244 [dsplinkk]
[ 131.929870] pc : [<bf0aa0c8>] lr : [<bf0aa074>] psr: 80000013
[ 131.929901] sp : c7fb5e28 ip : bf0b49f0 fp : c7fb5e8c
[ 131.941436] r10: bf0b6004 r9 : befdcf07 r8 : bf0b5ff8
[ 131.946685] r7 : 00000000 r6 : 31362e31 r5 : 00008000 r4 : bf0b4800
[ 131.953247] r3 : bf0b482c r2 : bf0b5ff8 r1 : befdcf07 r0 : 00000000
[ 131.959808] Flags: Nzcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
[ 131.967010] Control: 10c5387d Table: 87de4019 DAC: 00000015
[ 131.972778] Process messagegpp (pid: 1938, stack limit = 0xc7fb42e8)
[ 131.979156] Stack: (0xc7fb5e28 to 0xc7fb6000)
[ 131.983551] 5e20: 00000000 c7fb24c0 befdcc68 00000001 c04f9184 c04f904c
[ 131.991943] 5e40: c7fb5e5c c7fb5e50 bf0a7aa0 c04f9180 c7fb5e7c c7fb5e60 bf0b482c bf0b4800
[ 132.000335] 5e60: 00006f0c 00006c05 00008000 befdcc24 c7fb24c0 c003d004 c7fb4000 40024000
[ 132.008728] 5e80: c7fb5ef4 c7fb5e90 bf0ab46c bf0a9f94 c00b49fc c0057c54 c7e54c40 c7c42980
[ 132.017120] 5ea0: c7fb5ec4 00000000 c7d06a18 000844fb 40968000 c7fb24c0 c7fb5f34 00008000
[ 132.025512] 5ec0: 00000000 befdcf07 00000001 befdcc68 00010000 c7fb5ee0 c04facb4 c7fb24c0
[ 132.033874] 5ee0: 00006c05 befdcc24 c7fb5f14 c7fb5ef8 c00d0c50 bf0aaffc c7fb24c0 c7ced950
[ 132.042266] 5f00: befdcc24 c7fb24c0 c7fb5f7c c7fb5f18 c00d1294 c00d0be4 00000003 c7c42980
[ 132.050659] 5f20: 00087f30 00070000 c7fb5f74 c7fb5f38 c7fb5f64 c7fb5f40 c01e7c24 c0057c54
[ 132.059051] 5f40: c7fb4000 40968000 c7fb24c0 00000000 c7fb5f7c c7fb5f60 00000003 befdcc24
[ 132.067443] 5f60: 00006c05 c7fb24c0 c003d004 c7fb4000 c7fb5fa4 c7fb5f80 c00d1318 c00d0d74
[ 132.075836] 5f80: c7fb4000 00000001 00000792 00000000 00008bb4 00000036 00000000 c7fb5fa8
[ 132.084228] 5fa0: c003ce80 c00d12e4 00000792 00000000 00000003 00006c05 befdcc24 00000003
[ 132.092620] 5fc0: 00000792 00000000 00008bb4 00000036 00000000 00000000 40024000 befdcc0c
[ 132.101013] 5fe0: 00000000 befdcb40 0000b5e8 400f599c 20000010 00000003 00000000 00000000
[ 132.109405] Backtrace:
[ 132.111846] [<bf0a9f88>] (PMGR_PROC_load+0x0/0x244 [dsplinkk]) from [<bf0ab46c>] (DRV_Ioctl+0x47c/0x7d8 [dsplinkk])
[ 132.122589] [<bf0aaff0>] (DRV_Ioctl+0x0/0x7d8 [dsplinkk]) from [<c00d0c50>] (vfs_ioctl+0x78/0x94)
[ 132.131683] r6:befdcc24 r5:00006c05 r4:c7fb24c0
[ 132.136352] [<c00d0bd8>] (vfs_ioctl+0x0/0x94) from [<c00d1294>] (do_vfs_ioctl+0x52c/0x570)
[ 132.144714] r7:c7fb24c0 r6:befdcc24 r5:c7ced950 r4:c7fb24c0
[ 132.150421] [<c00d0d68>] (do_vfs_ioctl+0x0/0x570) from [<c00d1318>] (sys_ioctl+0x40/0x64)
[ 132.158691] r9:c7fb4000 r8:c003d004 r7:c7fb24c0 r6:00006c05 r5:befdcc24
[ 132.165283] r4:00000003
[ 132.167938] [<c00d12d8>] (sys_ioctl+0x0/0x64) from [<c003ce80>] (ret_fast_syscall+0x0/0x2c)
[ 132.176361] r7:00000036 r6:00008bb4 r5:00000000 r4:00000792
[ 132.182098] Code: e1a01009 e5936000 e51b3034 e1a00007 (e596c020)
[ 132.188385] ---[ end trace 3fad10b642e95a22 ]---
[ 133.147674] Unable to handle kernel NULL pointer dereference at virtual address 00000000
[ 133.156524] pgd = c0004000
[ 133.159271] [00000000] *pgd=00000000
[ 133.163391] Internal error: Oops: 817 [#2] PREEMPT
[ 133.168212] Modules linked in: lpm_omap3530 dsplinkk nls_iso8859_1 ircomm_tty ircomm irda
[ 133.176513] CPU: 0 Tainted: G D (2.6.29-omap1 #18)
[ 133.182403] PC is at exit_mmap+0x170/0x188
[ 133.186523] LR is at kmem_cache_free+0x20/0x68
[ 133.191009] pc : [<c00b3bcc>] lr : [<c00bf610>] psr: 20000113
[ 133.191009] sp : c7fd5de0 ip : c7fd5da8 fp : c7fd5e14
[ 133.202545] r10: 00000001 r9 : c7e404c0 r8 : 00000000
[ 133.207824] r7 : c7d969c0 r6 : 00000000 r5 : 00000061 r4 : c7d96b00
[ 133.214385] r3 : 00000000 r2 : 0000003f r1 : c7f80650 r0 : 00000000
[ 133.220947] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
[ 133.228118] Control: 10c5387d Table: 87da8019 DAC: 00000015
[ 133.233886] Process ipaq-sleep (pid: 1907, stack limit = 0xc7fd42e8)
[ 133.240295] Stack: (0xc7fd5de0 to 0xc7fd6000)
[ 133.244659] 5de0: c7fd5de8 00000000 0000004d c06a9c48 c7d969c0 00000000 c7d969c0 c7d969f4
[ 133.253051] 5e00: c7fd5ee0 c7fd5f60 c7fd5e2c c7fd5e18 c005dce4 c00b3a68 00000000 c7b4e9c0
[ 133.261444] 5e20: c7fd5e54 c7fd5e30 c0061cfc c005dcb4 c008bc00 c7fd4000 c7fd4000 c7b4e9c0
[ 133.269836] 5e40: 0000000b c7fd4000 c7fd5e74 c7fd5e58 c0063730 c0061bc4 0000000b 00000001
[ 133.278228] 5e60: 00000000 00000000 c7fd5e94 c7fd5e78 c0063e28 c00635d4 0000000b c7dc5030
[ 133.286621] 5e80: 000000dc c7fd4000 c7fd5ecc c7fd5e98 c006e164 c0063d84 c7fd5fb0 c7dc5040
[ 133.294982] 5ea0: c7fd5f3c 00000000 00000001 c7fd5fb0 beb98b4c 00000000 c7fd4000 000121cf
[ 133.303375] 5ec0: c7fd5fac c7fd5ed0 c003f17c c006dde0 c7fd5f3c 00000017 c00af8c4 c06681dc
[ 133.311767] 5ee0: 0000000b 00000000 00030001 00000000 c00423f0 c007a144 c7fd4000 00008000
[ 133.320159] 5f00: c003c220 c0042278 c7fd5f2c c7fd5f18 c01e7ab4 c0057c54 00010000 c7b4e9c0
[ 133.328552] 5f20: c7fd5f3c c7fd5f30 c007a148 c01e7a10 c7fd5f7c c7fd5f40 c0042470 c00421a4
[ 133.336944] 5f40: 00030001 c7fd5fb0 00000000 00000000 c7fd5f7c ffffffff 00000001 00000000
[ 133.345336] 5f60: beb98b4c 0000176b 00000001 000121cf c7fd5f9c c7fd5f80 c0042544 c0042278
[ 133.353698] 5f80: ffffffff ffffffff 00000001 00000000 beb98b4c 00000000 c7fd4000 000121cf
[ 133.362091] 5fa0: 00000000 c7fd5fb0 c003cecc c003f11c 00000000 00000000 00000000 00000010
[ 133.370483] 5fc0: 00018a50 00000001 00000000 beb98b4c 0000176b 00000001 000121cf 00000000
[ 133.378875] 5fe0: 00013180 beb98b34 0001311c 00000000 60000010 ffffffff 00000000 00000000
[ 133.387268] Backtrace:
[ 133.389709] [<c00b3a5c>] (exit_mmap+0x0/0x188) from [<c005dce4>] (mmput+0x3c/0xf4)
[ 133.397369] [<c005dca8>] (mmput+0x0/0xf4) from [<c0061cfc>] (exit_mm+0x144/0x14c)
[ 133.404937] r5:c7b4e9c0 r4:00000000
[ 133.408569] [<c0061bb8>] (exit_mm+0x0/0x14c) from [<c0063730>] (do_exit+0x168/0x7b0)
[ 133.416381] r7:c7fd4000 r6:0000000b r5:c7b4e9c0 r4:c7fd4000
[ 133.422119] [<c00635c8>] (do_exit+0x0/0x7b0) from [<c0063e28>] (do_group_exit+0xb0/0xdc)
[ 133.430267] [<c0063d78>] (do_group_exit+0x0/0xdc) from [<c006e164>] (get_signal_to_deliver+0x390/0x3e4)
[ 133.439758] r7:c7fd4000 r6:000000dc r5:c7dc5030 r4:0000000b
[ 133.445495] [<c006ddd4>] (get_signal_to_deliver+0x0/0x3e4) from [<c003f17c>] (do_notify_resume+0x6c/0x588)
[ 133.455230] [<c003f110>] (do_notify_resume+0x0/0x588) from [<c003cecc>] (work_pending+0x1c/0x20)
[ 133.464111] Code: e5973074 e3530001 9a000002 e3a03000 (e5833000)
[ 133.494750] ---[ end trace 3fad10b642e95a23 ]---
[ 133.500152] Fixing recursive fault but reboot is needed!
Could anyone please suggest me to proceed further........
Thanks and regards,
Sujay