Other Parts Discussed in Thread: DM3730, ADS7846, TVP5146M2
I use AM\DM37x EVM .I do not kown why the board can't work .I power on the board ,it can.t boot the system . when starting udev ,it always stops .
message :
Looking up port of RPC 100003/ on 202.193.52.10
Looking up port of RPC 100005/1 on 202.193.52.10
VFS: Mounted root (nfs filesystem) on device 0:12.
Freeing init memory: 172K
INIT: version 2.86 booting
Please wait: booting...
Starting udev