This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use McASP as McBSP in SITARA AM3892

Other Parts Discussed in Thread: AM3892

HI, IN sitara AM3892, there are 3 McASP but an single McBSp. i wanted to know how i can use the available McASP as McBSP. Kindly Help.

It is for non audio purpose.

  • Hi Akshay,

    I don't think you can use McASP for non audio purpose. From AM389x TRM:

    14.1.1 Purpose of the Peripheral
    The multichannel audio serial port (McASP) functions as a general-purpose audio serial port optimized for the needs of multichannel audio applications. The McASP is useful for time-division multiplexed (TDM) stream, Inter-Integrated Sound (I2S) protocols, and intercomponent digital audio interface transmission (DIT).

    What exactly you want to do with McASP ?

    Regards,

    Pavel


  • Hi Pavel,

    I am interfacing the AM3892 with two FPGAs. The ARM processor will hav complete control over the two FPGAs, i planned to interface the Arm and FPGA using McBSP, but since the processor contains only one McBSP, i wanted to know if i can interface the ARM processor to the 2nd FPGA using McASP which is configured as McBSP.

    Regards 

    Akshay

  • Hi Akshay,

    Here is some info on this topic:

    http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/216182.aspx

    http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/t/171412.aspx

    http://e2e.ti.com/support/dsp/sitara_arm174_microprocessors/f/791/t/195077.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/131194/473714.aspx

    Also, you can check into the AM389x TRM and Datasheet, and compare the McBSP vs McASP in term of supported features, internal architecture, registers, pins, etc.

    Regards,

    Pavel

  • Hi Pavel, 

    In one of the Links you sent, it says you can configure  the McASP as general purpose Serial port, this is contradicting to your 1st ans saying it cant be used for data other audio. Please clarify.

    Regards

    Akshay

  • Hi Akshay,

    In which link exactly is stated that McASP can be configured as general purpose serial port?

    The AM389x TRM is clear about that, McASP functions as a general purpose audio serial port. Per my understanding, you can interface McASP with external FPGA only with audio related data.

    Best Regards,

    Pavel