Hello all,
Can you please advise on if there is a performance degradation in this working method and if so, how can be minimized?
According to SPRUGU6 (sec1.2.1) if SYS_CLK>100 MHz or VDDEMIF=1.8V, the EM_SDCLK must be equal SYS_CLK/2.
In the design the SYS_CLK=150 MHz and VDDEMIF=1.8V, so EM_SDCLK=75MHz. Because of this status there are following questions:
- How is DSP performance (MIPS) degraded if ALL program memory is placed in external DPRAM and DPRAM is working at half SYS_CLK?
- If DSP performance is degraded significantly, what is your recommendation to minimize the degradation?
Thank you.
Regards,
Elina