This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Android ICS power on button

Hi,

 We are working with the AM/DM37X Evaluation module from Mistral and Android ICS 4.0.3. The powerOn button in the board effectively shutdown android. Once the system is shutdown we get the system halted message in the kernel console. But, we want to know how can we power on the module again using the same powerOn button that we used to shut it down. We know that this button is connected to the Power Module, wich generates an interrupt to power-button driver, which read the event through i2c and report the press of the button, but once the system is shut down and the kernel is halted, the interrupt doesn't work anymore.

I would really apreciate any help on this,

Regards,

Alberto Garcia