Can someone point me to the complete MPEG4 Encoder settings used to test performance as documented in the MPEG4 Encoder datasheet???
I am trying to determine why I cannot get any more than 8 fps. Even though the ARM/MJCP is running at 135 MHz as opposed to 216 MHz, I think I should be seeing frame rates in the neighborhood of 15+ fps.
My system has incoming 720p frames from a CMOS sensor. They travel through IPIPE and are stored directly to DDR in 422 format. (To save bandwidth, I do NOT capture raw frames to DDR, and then process them through IPIPE and back to DDR.)