This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High CPU usage when 3D Graphics Applications are running



Hi,

We are testing 3D Graphics performance for AM335X custom board with 4.3" LCD and

256MB DDR2 RAM. But we are suprised to usage of CPU.

When ChameleonMan is running, we see %95 CPU usage with top command. 

When 3D Navigation is running, we see %98 CPU usage with top command.

But all SGX libraries are installed correctly. Could you clarify this issue? Why CPU usage

is much more high when upper 3D applications are running?

Best Regards,

FERHAT YALDIZ