Hi,
We are using the latest version of the EZSDK 5_05_01_04.
Problem Faced: Audio gaps seen when we use arecord application to record Audio
eg: arecord -Dhw:0,0 -c 2 -f S16_LE -r48000 48KHz.pcm
The Audio is connected to LINE IN of the base EVM, Howewer we see Audio Gaps for other sampling frequency like 44100, 32000 also.
Almost 1-2 gaps are observed for a 5 min duration record.
It would be really helpfull if you can point out the problem related to the Audio Capture.
Regards,
Sudeep