Hi Guys!
We have sucessfully integrated the above mentioned threefive LCD panel with beagle bone through an expansion board. We selected this model because it was mentioned in porting guides and LCD7 cape on beagletoys also has this model installed.
The order to Europe is quite complicated and we want to find some alternatives with similar FFC interface but as another thread here on the forum describes there is nowhere a normal datasheet available for these threefive lcds models.
So in short. I'm searching on panelook.com and the threefive website says that these mentioned models are 7 inch 800x480 RGB interface with 60pins and 24 data bus.
On panel look there are several RGB interface description CPU/RGB, Paralell RGB, Serial RGB etc...
It would be great if someone could write me down what the conventions are to identify an LCD with similar hw characeteristics as the three five LCDS.
Another solution could be to select and LCD and make another expansion interface to fit that FFC but I want to select something close to these models, to avoid problems with porting.
Chipsee also had inegrated innnolux AT070TN92 LCD with beaglebone but I want a bit brighther LCD because it is only 250 cd/m2.
So in short I have pre-produced 10 expansion boards that fit TFC-S9700RTWV35/45 FFC interface. What do you recommend to search for compatible LCD interface or to pick a new LCD that is widely produced and supported by BeagleBone and to make a new expansion board design?
7 inch and 800x480 is important because I already have the housing design for my terminal... I need something that is sunreadable...
Thanks in advance for your hints,
best regards,
sodjas