Hello guys,
I'm trying to install a TMS320C5505 eZDSP on my laptop. I receive this fatals errors when im trying to connect it ('Target>Connect Target'):
first time:
"C55xx: Error connecting to the target: Error 0x80000240/-604 Fatal Error during: Initialization, OCS, "
then when i retry:
"C55xx: Error connecting to the target: Error 0x80002240/-121 Fatal Error during: Initialization, OCS, Control, "
I used dbgjtag.exe to find what's the explanation:
-the error 604 mean that the attent to load or install a required dynamic library failed
-the error 121:
"A bad controller handle has been given to a function
either before attempting to open the controller, or
having opened the controller and ignored its error s
Valid controller handles are generated when attempts
to open the controller return a clean error status."
I also checked the windows device manager and it seems that the device is not installed(device put in "other device" and error "The drivers for this device are not installed. (Code 28)")
So here i am :( , Is it a driver problem ? Or not ? What is that library dbgjtag is talking about ? Anybody know a solution?
thanks