Other Parts Discussed in Thread: AM1808, TSC2007
Dear Team,
I am try to porting tsc2007 to AM1808 in a customer board.
i getting the following error while booting.
tsc2007_init[382]
tsc2007_probe[272]
tsc2007 1-0090: i2c io error: -6
details added in board-da850-evm.c
#define DA850_EVM_TSC2007_ADDRESS 0x90
/*
* TSC 2007 Support
*/
#define TSC2007_GPIO_IRQ_PIN GPIO_TO_PIN(8, 12)
static int tsc2007_init_irq(void)
{
int ret = 0;
ret = gpio_request(TSC2007_GPIO_IRQ_PIN, "tsc2007-irq");
if (ret < 0) {
pr_warning("Failed to Set TSC2007 IRQ GPIO: %d\n", ret);
return ret;
}
ret = davinci_cfg_reg(DA850_GPIO8_12);
if (ret) {
pr_warning("%s: PinMux setup for GPIO %d failed: %d\n",
__func__, TSC2007_GPIO_IRQ_PIN, ret);
return ret;
}
gpio_direction_input(TSC2007_GPIO_IRQ_PIN);
return ret;
}
static void tsc2007_exit_irq(void)
{
gpio_free(TSC2007_GPIO_IRQ_PIN);
}
static int tsc2007_get_irq_level(void)
{
return gpio_get_value(TSC2007_GPIO_IRQ_PIN) ? 0 : 1;
}
struct tsc2007_platform_data tsc2007_pdata = {
.model = 2007,
.x_plate_ohms = 180,
.get_pendown_state = tsc2007_get_irq_level,
.init_platform_hw = tsc2007_init_irq,
.exit_platform_hw = tsc2007_exit_irq,
};
static struct i2c_board_info __initdata da850_evm_tsc2007_dev = {
I2C_BOARD_INFO("tsc2007", DA850_EVM_TSC2007_ADDRESS),
.platform_data = &tsc2007_pdata,
};
i2c_register_board_info(1, da850_evm_i2c_devices,
ARRAY_SIZE(da850_evm_i2c_devices));
da850_evm_tsc2007_dev.irq = gpio_to_irq(TSC2007_GPIO_IRQ_PIN),
i2c_register_board_info(1, &da850_evm_tsc2007_dev, 1);
Please help me resolve to this issue.
Regards
Jithin