This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mDDR reading and writing problem with AM335x

I have followed the tips,followed the caculate tools, seed spreadsheet. but still got the problem

the following is the picture of the momery. The red indicates the changed(because I have enable the continuous refresh) ,the address changed was randomized,

And if Changed the value of somewhere, the value of other place may be changed, this is what i saw.

in the tips, there are two cases between DDR_CK length and DDR_DQS length, but what will be result if DDR_CK length equal to DDR_DQS length?

Btw, I try to use different SDRAM drive strength, see the following picture:

FULL drive strength:

1/8 drive strength:

I have write the 0x12345678 to 0x80000000 and 0xdeadbeef to 0x8000000C.

the red shows the change between a second before, I think FULL drive strength may be better than 1/8 drive strength,  because in am335x-evm, after initial the DDR2, the contents are different each other,it couldn't be 0xFF mostly.

Could you give any advice?

Thanks.