Hi,
I am facing a problem when omapl138 is connected to monitor through vga port.I just able to see a TI logo displaying on the screen and that's all nothing else.
Do I need to configure my board ?? anyone facing the same problem??Please help me..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am facing a problem when omapl138 is connected to monitor through vga port.I just able to see a TI logo displaying on the screen and that's all nothing else.
Do I need to configure my board ?? anyone facing the same problem??Please help me..
Hi,
Which software is running on the board?
Do you have any debug info related to this?
-Regards,
Balaji N
Hi,
Do I need to change any switch positions on the board,to enable vga display?
Thank you ,
venkatesh.
This is normal and to indicate that Linux is up and running and FBDev is working showing the TI logo. You can test FBdev by transferring a 640x480 bitmap file to LCDK (using the 'scp' command as in the 'hello world' example in the Getting Started Guide) or if you are using NFS mount then just 'sudo cp' the file to the ;/home/root' folder.
Once the bitmap file is there, execute 'fbsplash -s <image file name> to see it displayed.
LCDK SDK provides the tools to implement Linux applications using GStreamer, Qt, ALSA, thttpd APIs as well as TI Syslink API to interface to a program running on the DSP where it can be used to do some number crunching. Consult the Software Developers Guide to have the TI tools installed and run the Syslink examples to see how message and data can be passed between Linux and DSP for processing.
Hi,
I transfered many (black n white as well as color) 640X480 bitmap image to home/root/ folder of LCDK,and executed "fbsplash -s <image_name.bmp>".
There is a error message showing: fbsplash: bad PPM file 'our_image_rgb.bmp' .
Please sort out the problem.
Thank you,
venkatesh.
Hi Venkatesh,
The error you are specifing fbsplash: bad PPM file 'our_image_rgb.bmp' arises as the fbsplash utility checks for the ppm file as input but you are giving a bitmap file.
You can do this in a slightly different way. You can convert your .bmp file into .ppm file using the linux command line utility bmptoppm and then proceed with the fbsplash command and you can see the image in your VGA display.
NOTE:The bmptoppm is one type of converter in the package netpbm (package of graphics manipulation programs and libraries).
Thanks
Iyshwarya
If this answers your question, please click the Verify Answer button below. If not, please reply back with more information