Hi Biser,
The TRM of AM335x show its maximum SD Speed is 24MB/S. But the Micro SD card speed class(2,4,6,10,UHS Speed Class1) only define its minimum transfer speed. I am still confused after I searched the topic about the Micro SD card.
And it seems there are four types of Micro SD card: microSD, microSDHC, microSDXC, UHS-I Cards.
Pls help confirm which type and which class Micro SD card can be used on AM335x for booting ROM.
I found one TI employee mentioned one SanDisk extreme high speed card as below picture. Which kind of Micro SD card is it?
http://e2e.ti.com/support/dsp/sitara_arm174_microprocessors/f/791/t/195143.aspx
Best regards,
Cosmo