Hi,
Posted in StarterWare but no answer there, so lets hope here it could be answered.
I've succesfully installed the StarterWare for L138 LCDK and with the usage of a XDS100v2 I can have JTAG access to the LCDK.
So, now I'm trying to have a debug run of the 'demo' that is provided in the StarterWare, which is this one
-> OMAPL138_StarterWare_1_10_03_03\examples\lcdkOMAPL138\demo
I'm connecting a VGA monitor on the VGA LCDK connector and starting the CCS debug session.
The initialization script goes ok as it seems
ARM9_0: Output: Target Connected.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: Memory Map Cleared.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: Memory Map Setup Complete.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: PSC Enable Complete.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: PLL0 init done for Core:300MHz, EMIFA:25MHz
ARM9_0: Output: DDR initialization is in progress....
ARM9_0: Output: PLL1 init done for DDR:150MHz
ARM9_0: Output: Using DDR2 settings
ARM9_0: Output: DDR2 init for 150 MHz is done
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: DSP Wake Complete.
ARM9_0: Output: ---------------------------------------------
and when I start execution I got on the VGA screen output from the application and six icons from which I guess I have to choose one.
At that time, the application waits for my input, yet altough I tried to connect a USB mouse, it did not show up on the screen.
How can I have a mouse connected and activated in the board or what input does the 'demo' example in L138 LCDK StarterWare wants?
Any help on how to run this demo is appreciated since I could not see any text accompanying it.
Christos