Other Parts Discussed in Thread: AM3359
Hi
I am using Sitara AM3359 processor,Now i planned to interface a capacitive 3.5" inch touchscreen with the processor.In the processor datasheet,it has an inbuilt LCD CONTROLLER & Touch-Screen Controller.Then How do i know it is suitable for Resistive & capacitve TFTs because Resistive needs ADC pins and capacitive TFTs needs I2C pins from processor.
In EVM-SK kit they use 4.3" capacitive (Newhaven display) display,but how do i know,it is applicable for both resistive & capacitive TFTs from processor(datasheet) itself??
Thanks in advance