Hi,
I am using TMS320DM6467 Evaluation module.
I am using bootargs as follows:
EVM # setenv bootcmd 'nboot 80700000 0 a0000;bootm'
EVM # setenv bootargs mem=120M console=ttyS0,115200n8 root=/dev/hda1 rw noinitrd ip=dhcp davincihd_capture.channel0_numbuffers=4
EVM#saveenv
EVM#boot
and the boot log is as follows.
Starting kernel ...
Uncompressing Linux............................................................................................... done, boo.
Linux version 2.6.10_mvl401-davinci_evm-PSP_01_30_00_082 (x0096290@linwoodxc22) (gcc version 3.4.3 (MontaVista 3.4.3-25.0.248
CPU: ARM926EJ-Sid(wb) [41069265] revision 5 (ARMv5TEJ)
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Machine: DaVinci DM6467 EVM
Memory policy: ECC disabled, Data cache writeback
DM6467
Built 1 zonelists
Kernel command line: mem=120M console=ttyS0,115200n8 root=/dev/hda1 rw noinitrd ip=dhcp davincihd_capture.channel0_numbuffer4
PID hash table entries: 512 (order: 9, 8192 bytes)
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 118528KB available (2379K code, 513K data, 164K init)
Mount-cache hash table entries: 512 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
spawn_desched_task(00000000)
desched cpu_callback 3/00000000
ksoftirqd started up.
desched cpu_callback 2/00000000
desched thread 0 started up.
NET: Registered protocol family 16
DaVinci: 48 gpio irqs
Registering platform device 'serial8250.0'. Parent at platform
Registering platform device 'musb_hdrc'. Parent at platform
DaVinci I2C DEBUG: 20:15:30 Jun 20 2008
Registering platform device 'i2c'. Parent at platform
ch0 default output "COMPOSITE", mode "NTSC"
ch1 default output "", mode ""
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
musb_hdrc: version 2.2a/db-0.4.8 [cppi-dma] [host] [debug=0]
musb_hdrc: ConfigData=0x06 (UTMI-8, dyn FIFOs, SoftConn)
musb_hdrc: MHDRC RTL version 1.500
musb_hdrc: USB Host mode controller at c8000000 using DMA, IRQ 13
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
JFFS2 version 2.2. (NAND) (C) 2001-2003 Red Hat, Inc.
yaffs Jun 20 2008 20:15:06 Installing.
Registering platform device 'DavinciHD_vdce.2'. Parent at platform
CIR device registered successfully (Major = 253, Minor = 0)<6>Registering platform device 'cir.0'. Pam
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
Registering platform device 'serial8250'. Parent at platform
ttyS0 at MMIO 0x1c20000 (irq = 40) is a ST16654
ttyS1 at MMIO 0x1c20400 (irq = 41) is a ST16650V2
io scheduler noop registered
io scheduler anticipatory registered
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Registering platform device 'ti_davinci_emac'. Parent at platform
TI DaVinci EMAC: MAC address is 00:0e:99:02:b5:c6
TI DaVinci EMAC Linux version updated 5.0
TI DaVinci EMAC: Installed 1 instances.
netconsole: not configured, aborting
i2c /dev entries driver
Linux video capture interface: v1.00
Registering platform device 'vpif capture.1'. Parent at platform
Registering platform device 'vpif display.1'. Parent at platform
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
MUX: initialized ATAEN
hda: TOSHIBA MK4032GAX, ATA DISK drive
elevator: using anticipatory as default io scheduler
ide0 at 0xe10661f0-0xe10661f7,0xe10663f6 on irq 22
hda: max request size: 1024KiB
hda: 78140160 sectors (40007 MB), CHS=16383/255/63
hda: hda1 hda2
ide0: BM-DMA at 0xe1066000-0xe1066007, BIOS settings: hda:pio, hdb:pio
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
Registering Audio Devices. Total communication peripherals (ASP) : 2
Codec with ID = 0 on ASP = 0 is initialized.Using minor number : 3
Configuring the McASP as Master
Configuring the McASP 1 for DIT
SPDIF on ASP = 1 isinitialized.Using minor number : 19
NET: Registered protocol family 2
IP: routing cache hash table of 512 buckets, 4Kbytes
TCP: Hash tables configured (established 8192 bind 16384)
NET: Registered protocol family 1
NET: Registered protocol family 17
Sending DHCP requests ...... timed out!
IP-Config: Reopening network devices...
Sending DHCP requests ...... timed out!
IP-Config: Auto-configuration of network failed.
kjournald starting. Commit interval 5 seconds
EXT3-fs warning: maximal mount count reached, running e2fsck is recommended
EXT3 FS on hda1, internal journal
EXT3-fs: recovery complete.
EXT3-fs: mounted filesystem with ordered data mode.
VFS: Mounted root (ext3 filesystem).
Freeing init memory: 164K
INIT: version 2.85 booting
Mounting a tmpfs over /dev...done.
Creating initial device nodes...done.
Activating swap...done.
Remounting root filesystem...done.
Calculating module dependencies
WARNING: Couldn't open directory /lib/modules/2.6.10_mvl401-davinci_evm-PSP_01_30_00_082: No such file or directory
FATAL: Could not open /lib/modules/2.6.10_mvl401-davinci_evm-PSP_01_30_00_082/modules.dep.temp for writing: No such file or y
Loading modules:
Checking all file systems: fsck
fsck 1.35 (28-Feb-2004)
Mounting local filesystems: mount modprobe: FATAL: Could not load /lib/modules/2.6.10_mvl401-davinci_evm-PSP_01_30_00_082/moy
mount: fs type relayfs not supported by kernel
failed (32: ).
Cleaning: /tmp /var/lock /var/run done.
Setting up networking (ifupdown) ..
Cleaning: /etc/network/run/ifstate done.
Starting network interfaces: done.
Starting hotplug subsystem:
pci
pci [success]
usb
usb [success]
isapnp
isapnp [success]
ide
ide [success]
input
input [success]
scsi
scsi [success]
done.
Starting portmap daemon: portmap.
done.
Setting pseudo-terminal access permissions...done.
Updating /etc/motd...done.
INIT: Entering runlevel: 3
Starting NFS common utilities: statd lockd.
Starting internet superserver: inetd.
in rcd...
CMEMK Error: CMEM phys_start (0x87600000) overlaps kernel (0x80000000 -> 0x87800000)
insmod: error inserting 'cmemk.ko': -1 Invalid parameters
dsplinkk: no version for "struct_module" found: kernel tainted.
dsplinkk: module license 'DSP/BIOS(TM) LINK' taints kernel.
DSPLINK Module (1.50) created on Date: Jan 3 2008 Time: 13:16:55
Starting web server ...
thttpd
DVT-DSA proc module 1.0 initialized
modprobe: FATAL: Could not load /lib/modules/2.6.10_mvl401-davinci_evm-PSP_01_30_00_082/modules.dep: No such file or directoy
modprobe: FATAL: Could not load /lib/modules/2.6.10_mvl401-davinci_evm-PSP_01_30_00_082/modules.dep: No such file or directoy
Starting MontaVista target tools daemon: mvltdmvltd version 2.1 MontaVista Software,Inc.
mvltd[1132]: can't send broadcast message: Network is unreachable
mvltd[1132]: can't send broadcast message: Network is unreachable
mvltd[1156]: started on port 34577
.
MontaVista(R) Linux(R) Professional Edition 4.0.1 (0600980)
(none) login: root
Last login: Thu Jan 1 00:12:19 1970 on console
Linux (none) 2.6.10_mvl401-davinci_evm-PSP_01_30_00_082 #1 Fri Jun 20 20:17:18 IST 2008 armv5tejl GNU/Linux
Welcome to MontaVista(R) Linux(R) Professional Edition 4.0.1 (0600980).
root@(none):~#
During booting time it is waiting requests. But I want to boot it from hard disk file system alone.
After a while it is booting from Hard disk only.
Is there issue in boot sequence.?
And I want to copy my applications which were built on host through TFTP.
Please suggest me how Can I proceed further.
Waiting for quick response..
Thanks in advance.