Hello All,
1.In our prototype board we have connected one lane of Antenna Interface AIF2(from DSP to SFP) (one transmitter and one receiver) to SFP connector.Is the any constraint on the no. of lanes to be connected? Our intention is to deliver the CPRI frame created by AIF2 to RRH.
2.if we proceed with one lane what is the data rate that can be achieved?
3.1Gbps 20kms range SFP Connectors are available with us(reason for using 1 lane).Can we proceed?