Other Parts Discussed in Thread: OMAP-L138
Hi,
I am using OMAP-L138 EVM board - Kernel version 2.6.37. By default kernel compression mode is selected as gzip format. But when I try to change the compression format to LZO. I am getting compilation error as given below:
make[1]: Entering directory `/home/ti-dvsdk_omapl138-evm_04_03_00_06/psp/linux-2.6.37-psp03.21.00.04.sdk'
CHK include/linux/version.h
CHK include/generated/utsrelease.h
make[2]: `include/generated/mach-types.h' is up to date.
CALL scripts/checksyscalls.sh
CHK include/generated/compile.h
GZIP kernel/config_data.gz
IKCFG kernel/config_data.h
CC kernel/configs.o
LD kernel/built-in.o
LD vmlinux.o
MODPOST vmlinux.o
WARNING: modpost: Found 2 section mismatch(es).
To see full details build your kernel with:
'make CONFIG_DEBUG_SECTION_MISMATCH=y'
GEN .version
CHK include/generated/compile.h
UPD include/generated/compile.h
CC init/version.o
LD init/built-in.o
LD .tmp_vmlinux1
KSYM .tmp_kallsyms1.S
AS .tmp_kallsyms1.o
LD .tmp_vmlinux2
KSYM .tmp_kallsyms2.S
AS .tmp_kallsyms2.o
LD vmlinux
SYSMAP System.map
SYSMAP .tmp_System.map
OBJCOPY arch/arm/boot/Image
Kernel: arch/arm/boot/Image is ready
LZO arch/arm/boot/compressed/piggy.lzo
/bin/sh: lzop: command not found
make[3]: *** [arch/arm/boot/compressed/piggy.lzo] Error 1
make[2]: *** [arch/arm/boot/compressed/vmlinux] Error 2
make[1]: *** [uImage] Error 2
make[1]: Leaving directory `/home/ti-dvsdk_omapl138-evm_04_03_00_06/psp/linux-2.6.37-psp03.21.00.04.sdk'
make: *** [linux] Error 2
Please help me??? Thanks in advance...