This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Level in H264 decoder

Guru 20755 points

Hello,

H264 decoder for DM8168 is presetLevelIdc for configuring Level of codec.
I would like to ask why is this required when the decoder already can retrieve the given stream parameters from sequence header.
I also do not find this in MPEG4 decoder, or MPEG2 decoder.
Should it always be set to maximum level ?

Best Regards,

Ran