This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to disable the trace of the Codec Engine,NO_TRACING is not work

How to disable the trace of the Codec Engine in GPP application.The tarce information is as follow:

@0x090252b2:[T:0x41400490] CV - VISA_call(visa=0x59cb8, msg=0x42576880):
messageId=0x000206a8, command=0x1
@0x09025401:[T:0x41400490] CV - VISA_call Completed: messageId=0x000206a8, command=0x1,
return(status=0)
@0x09025420:[T:0x41400490] CV - VISA_freeMsg(0x59cb8, 0x42576880): Freeing message with
messageId=0x000206a8
@0x0902543f:[T:0x41400490] CV - VISA_getMaxMsgSize(0x59cb8): returning 0x1000
@0x0902545d:[T:0x41400490] CV - VISA_allocMsg> Allocating message for messageId=0x000206a9
@0x0902547c:[T:0x41400490] CV - VISA_call(visa=0x59cb8, msg=0x42576880):
messageId=0x000206a9, command=0x0
@0x090294db:[T:0x41400490] CV - VISA_call Completed: messageId=0x000206a9, command=0x0,
return(status=0)

......

I have set TraceUtil.attrs = TraceUtil.NO_TRACING in the .cfg file, but it doesn't work,the
trace information is still printed.

Who can help me?

DVSDK version 4.02

BR

Shenshilv