hi,
there is something wrong with repo. i got the below issue.
administrator@Lenovo:~$ curl https://dl-ssl.google.com/dl/googlesource/git-repo/repo > ~/bin/repo
% Total % Received % Xferd Average Speed Time Time Time Current
Dload Upload Total Spent Left Speed
0 0 0 0 0 0 0 0 --:--:-- 0:04:00 --:--:-- 0curl: (7) Failed to connect to 2404:6800:4008:c01::5d: Network is unreachable
but it could work several weeks ago.
do u meet it?
BR
Younger