This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6746 McBSP bit reversal problem



Hello,

I tried McBSP receive 32-bit reversal on C6746 device.

but, I can not receive 32-bit element(LSB first). (Actual received data are all 0.)

As expected, the transmitting side is reversed.

My register settings are shown below(According to the document[23.2.5.5.7 32-Bit Bit Reversal: RWDREVRS, XWDREVRS](SPRUH80A) ):

 RCR = 0x00A80FB0

  XCR = 0x00A80FB0

  SPCR = 0x02230027

Howerver, RCR.RCOMPAND = 0 and RCR.RWDREVRS = 1, I can receive 32-bit reversed data.

The above settings is correct ?

regards,

Chii