Hi,
I am using MISTRAL EVMOMAP3530 REV G board for programming ehci drivers.Even after initializing the usb clock the usb registers are not enabled.
The gel files does the following initialization
Cortex_A8_0: GEL Output: SystemClock = 19.2 MHz
Cortex_A8_0: GEL Output: DPLL_MULT_VALUE = 242
Cortex_A8_0: GEL Output: DPLL_DIV_VALUE = 13
Cortex_A8_0: GEL Output: CORE_DPLL_CLK = 663.771 MHz
Cortex_A8_0: GEL Output: CORE_CLK = 331.8855 MHz
Cortex_A8_0: GEL Output: L3_CLK = 165.9427 MHz
Cortex_A8_0: GEL Output: System Reset has occured.
I have enabled usb INTERFACE CLOCK and FUNCTIONAL CLOCK which is 120 MHz. Is there anything else to be done apart from this for echi initialization.
I am programming hsusb2.