This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WIFI WG7311 issue with AM335x processor

Other Parts Discussed in Thread: WL1271

Hi,

I do have an issue with the wifi module WG7311 with an inbuilt WL1271 WIFI module  being interfaced with AM335x processor

Issue: the Wifi_interrupt and WIFI_enable nt synching with each other.

The enable pin is driven out from the processor AM335x  into the WIFI module WG7311 via a level translator TXS108E.

whereas the interrupt pin is driven out from the wifi module WG7311 into level translator TXS108E input line ,then driven out to an  I2c expander input driving the I2c bus (SCL AND SDA lines) at its output lines.

Regds

Melisha.

  • Hi

    I am also using the same WiFi with above processor but I am unable to establish wlan0. I am using am335x evm reference and converted to our customized design. But we are using the WLAN with the same design of am335x even. Please help me how to bring up the WLAN.

    Thanks,

    lofna