Other Parts Discussed in Thread: SYSBIOS
Hi,
I am using the Timer 4 for the SYS/BIOS and I can observe that the Time is 10% faster as should be.
before I was using the 32kHz and it was not accurate !!
Is these issue known or maybe solved in the new SYS/BIOS version ?
SYSBIOS_ROOT := c:/ti/bios_6_33_04_39
XDC_ROOT := c:/ti/xdctools_3_23_03_53
/* Start DMTimer 4 manually and configure it to have 20MHz input clock */
/* the selection of 20MHz input clock is done in main.c */
var MyDMTimer = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');
MyDMTimer.intFreq.lo = 20000000; //20Mhz
MyDMTimer.intFreq.hi = 0;
kind regards
Mesut