This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Burning Ethernet App into NOR flash



Hello all,

I have a Logic PD evmomapl138 and CCSv5, Spectrum Digital jtag sd560v2. I am trying to burn into NOR flash an ethernet application. I have already done the led example and have been successful. I am using the configuration attached to load into the AISgen tool. I am using the ARM .out file included in that example to wake up the DSP. And am using my own .out DSP file. Now, the problem is that the application is not working when burnt. It does work when ran using the jtag debug mode. I've been searching thru your threads and did try some things suggested to others but have not been able to be successful. I downloaded the debug gel file and ran the diagnostics and found in the descriptions that the DSP has been put to sleep. I don't know if there is something missing in my configuration that is different for an ethernet echo application  than that of the led example. I did include 5 in the LPSC1 which corresponds to EMAC in the gel file.

Cfg file:

Boot Mode=NOR Flash
Boot Speed=115200
Flash Width=1
Flash Timing=3ffffffc
Configure Peripheral=True
Configure PLL0=True
Configure SDRAM=False
Configure PLL1=True
Configure DDR2=True
Configure LPSC=True
Configure Pinmux=True
Enable CRC=False
Specify Entrypoint=False
Enable Sequential Read=False
Use 4.5 Clock Divider=False
Use DDR2 Direct Clock=False
Use mDDR=True
ROM ID=3
Device Type=0
Input Clock Speed=24
Clock Type=0
PLL0 Pre Divider=1
PLL0 Multiplier=19
PLL0 Post Divider=1
PLL0 Div1=1
PLL0 Div3=5
PLL0 Div7=12
PLL1 Multiplier=25
PLL1 Post Divider=2
PLL1 Div1=1
PLL1 Div2=2
PLL1 Div3=3
Entrypoint=0
SDRAM SDBCR=0
SDRAM SDTMR=0
SDRAM SDRSRPDEXIT=0
SDRAM SDRCR=0
DDR2 PHY=c4
DDR2 SDCR=2034622
DDR2 SDCR2=0
DDR2 SDTIMR=1c923208
DDR2 SDTIMR2=3811c700
DDR2 SDRCR=c0000492
LPSC0 Enable=15
LPSC0 Disable=
LPSC0 SyncRst=
LPSC1 Enable=
LPSC1 Disable=
LPSC1 SyncRst=
Pinmux=4:2200+
App File String=
AIS File Name=

Any input will be greatly appreciated.

Thank you,

Michelle

  • Michelle,

    Thank you for going through the forums before posting your query here. When you ran the debug gel file, did you see the program counter at an address inside ROM or has the boot process completed with your application loaded in external memory and PC pointing to some location in your code.DSP has been put to sleep indicates to me that the ARM UBL didn`t bring the DSP out of reset correctly.

    Is there any memory map over lap in the DSP.out and the ARM ubl that is bringing up the DSP.? Is your DSP address aligned to 1024 bytes as described on the wiki for the led blink example?

    Regards,

    Rahul

  • Hello Rahul,

     

    Ok, so the PC is pointing to the code inside my code inside the main.  I have placed my entrypoint in 0x80000000 in the arm ubl and in the DSP's cdm. When I have the debug gel file running on the targets and I press the reset button I can see how the arm says there is a target reset but the dsp remains suspended.

     

    Michelle