This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uPP clock activation



Hi,

I'm using an OMAPL138-processor, PSP-driver (01.30.01) and DSP/BIOS (5.41.11.38).

Is it possible to activate ONLY the clock output of upp-channel B when the channel A is already configured in 16-bit RCV mode?

When I configure channel B in xmt-mode, for sure, I get the clock but the problem is, that channel A uses now also the XDATA-pins instead of the DATA pins and these pins are not outrouted on my board.

 

would be glad to get any informations about that.

thanks in advanced.

Christian