This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error in Debug Session in Am-1808 with CCS and Black Hawk USB 100 V2



Hi,

I have Am-1808 and i am following this guide to launch debugging session. I am using CCS V5 and Black-hawk USB 100 V2, While configuring targetconfiguration.ccxml i used "Texas Instruments XDS100v2 USB Emulator" as "Connection", since in the list Black Hawk USB 100 V2 was not listed. When i launch the debug session i get this error:

ARM9_0: Output: Memory Map Cleared.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: Memory Map Setup Complete.
ARM9_0: Output: ---------------------------------------------
ICEPICK_C: Error: (Error -150 @ 0x0) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 5.0.747.0)
ARM9_0: Error: (Error -1029 @ 0x2B5F) Invalid data read from ICECrusher register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.747.0)
ICEPICK_C: Power Failure on Target CPU
ARM9_0: Error: Failed to get PRSC status
ICEPICK_C: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging

Can u please tell what could be the issue ? And how can i resolve this ?

Thanks

Regards

Usama