Hello,
I am developing an application that contains Ethernet and SPI0 communication channels.
SPI0 pins are mutiplex with part of Ethernet pins.
Can I use SPI0 and Ethernet channels simultaneously?
Sincerely,
Yacob Hassidim.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am developing an application that contains Ethernet and SPI0 communication channels.
SPI0 pins are mutiplex with part of Ethernet pins.
Can I use SPI0 and Ethernet channels simultaneously?
Sincerely,
Yacob Hassidim.
Hi Yacob,
We have a pin multiplexing utility that can help you keep track of what functionality can be used together on a device. I have linked that tool below. Let us know if it helps resolve your issue or if you have any further questions.
OMAP-L132/L138, TMS320C6742/6/8 Pin Multiplexing Utility:http://www.ti.com/lit/pdf/sprab63
Thanks,
Clinton
Hello Clinton,
Thank you for your answer.
I use the development kit: TMS320C6740 DSP. See http://www.ti.com/tool/tmdxlcdk6748?DCMP=dsp-c6-lcdk-120524&HQS=c6748lcdk
Can I use the SPI0 channel on this development kit?
Can I use the SPI0 and Ethernet channels simultaneously on this development kit?
Can I use UART0/UART1 and Ethernet channels simultaneously on this development kit?
Sincerely,
Yacob Hassidim.