Other Parts Discussed in Thread: TVP5158
Our main goal is to capture video simultaneously from two composite inputs,encode in H264 format and display both videos simultaneously on onchip HDMI output.
ezsdk used: 5.05.01.04
target evm used : 8168 evm
IO board used : Dm816x video security board
Questions:
1. Is the above goal achievable?
2. I see two capture examples in the current sdk capture_encode_a8host_debug(OMAX) and saLoopBack which captures video from component input on the expansion I/O daughter card. Can you please throw some light on difference between these two examples?
3. Can the examples mentioned above be modified to accept composite input using TVP5158 decoder?
4. I donot see tvp5158 decoder driver in the current SDK. Can anyone please provide me with details or a patch on how to modify the current ezsdk applications to capture video from SD inputs via tvp5158 ?
Thanks,
Shilpa.