Hai
I get the reference design from am335x starter kit(TMDSSK3358),In that design they were using TPS65910 PMIC
In the power management chip,SDA_SDI (pin no-8),SCL_SCK (pin no-9) were used in SK kit integrated with am335x and leaving SDASR_EN2 (pin no-10) SCLSR_EN1(pin no - 11) as DNI pin without connecting to the host processor.But in am335x EVM kit,They were using pin 10,11 in PMIC leaving pin 8,9 as DNI.
Both the I2C pins were same??what the exact fuction of smart reflex in thjis place????Which I2C pis were could i use in my development board????